2024-11-26 6:23 AM
Hi,
I am working on a LoRa application with the STM32WL5MOC module which features the STM32WL55JC microcontroller. According to the datasheet, this module is compatible with a voltage level as low as 1.8V.
I am using the STM32CubeWL MCU Package for the firmware, and I have configured the Low Power (LP) mode for a 14dBm transmission power. However, the board stops functioning whenever the voltage drops below 2.05V.
Has anyone encountered a similar issue or have any suggestions on how to address this?
Thanks in advance!
2024-11-26 6:32 AM - edited 2024-11-26 6:59 AM
@SMav wrote:the board stops functioning whenever the voltage drops below 2.05V.!
What, exactly, do you mean by "stops functioning" ?
What board is this on?
PS:
Are you using VREFBUF:
2024-11-26 8:08 AM
Hello @SMav and welcome to the ST Community.
Could you please give more details about this behavior, your configuration, your design... it should be really helpful for our users to help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-27 4:38 AM - edited 2024-11-27 4:40 AM
Hi,
Thanks for the replies.
It is STM32WL STMod+ expansion board https://www.st.com/resource/en/schematic_pack/mb1779-high-band-b02-schematic.pdf
@Andrew Neil VREFBUF is disabled. RF stops transmitting when the supply voltage level is below 2.05V and I need to work with 1.8V for my application.
The hardware changes are as below:
Component | Modification | Description / comment |
C1, C8, C14, C17 | Fitted 4.7uF | bulk decoupling |
C2, C12, C15, C16 | Fitted 100nF | decoupling |
CN5 | 2 pin header fitted | Used to power the board |
JP2 | fitted | to pass through power to module |
U1 | removed | RF switch |
U2 | removed | accel / gyro |
U4 | removed | barometer |
U5 | removed | RF switch |
U6 | removed | LDO 3v3 |
U7 | removed | magnetometer |
U8 | removed | eeprom |
U10 | removed | serial flash |
R12 | shorted | set LP mode |
R15 | shorted | set LP mode |
SB35 | shorted | allow external supply |
SB14 | removed | disconnect onboard 3V3 |
Does anyone have any suggestions?
Thanks in advance!
2024-12-04 3:00 AM
Hey all,
Does anyone know a solution? Am I missing a step? Any help or suggestions would be greatly appreciated.
2024-12-04 3:14 AM
@SMav wrote:It is STM32WL STMod+ expansion board https://www.st.com/resource/en/schematic_pack/mb1779-high-band-b02-schematic.pdf
Maybe it's a limitation of that board - rather than the chip itself?
2024-12-04 4:40 AM
All hardware from the board that could affect the module's behaviour at lower voltages has been removed, so the module is essentially isolated. This means it is the module itself and not other hardware on the board. The changes to the hardware are mentioned above.