cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL54 does not wake up after 4-5 days in STOP2 mode

euclid
Associate

The device is designed i  a way that, it should wake up every 30 seconds via RTC wake up timer or upon button press, read sensor values (for temperature and humidity ), if there is any change in these values , send packets via radio (SUBGhz) and enter STOP 2 mode. 

This works for 3-4 days after which it does not wake up.

The radio core is held in reset before entering STOP 2 mode. 

 

 

1 REPLY 1
Sarra.S
ST Employee

Hello @euclid

There are many potential causes, could you share with us more details (EXTI config, RTC config), the radio core is it correctly re-initialized after waking up? 

Also, consider using a watchdog timer to reset the microcontroller if it gets stuck, and add logging or debugging information to track the state of the microcontroller over time 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.