cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575: overconsumption in stop2 with LPUART DMAT set

nicolas
Senior II

I have an overconsumption of ~50uA when going into stop2 mode with the DMAT of LPUART set.

Because of the silicon bug (LPUART does not generate DMA requests after setting/clearing DMAT bit), I can't easily clear this flag (the workaround can lead to loss of rx data).

It's probably related to:

https://community.st.com/t5/stm32-mcus-products/hal-pwrex-entershutdownmode-not-working-due-usart-dmarequests-sw/m-p/51367

2 REPLIES 2
Sarra.S
ST Employee

Hello @nicolas

If clearing DMAT is necessary, after the end of DMA transfers, once DMAT is cleared, disable and re-enable the peripheral through the UE bit of the USART_CR1 register. This workaround is acceptable only if the peripheral is not used in receiver mode

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I can't use the workaround because I need to always stay in rx.

Perhaps the best solution is to use DMA for rx only and to use interrupt for the tx which is less time critical.