2026-05-08 2:12 AM - last edited on 2026-05-08 3:48 AM by Imen.D
We have a custom `STM32WL33CCV6` (`VFQFPN32`) board that should reach about `4 µA` in Deepstop, similar to the NUCLEO-WL33, but instead it drops only to roughly `450–500 µA` and appears to restart on Deepstop entry. `NRST` does not glitch low, and the behavior is unchanged with only `3.3V` and `GND` connected. We also tested direct `HAL_PWR_EnterDEEPSTOPMode()` with wake sources disabled, and it still appears to reboot rather than stay in Deepstop.
We reviewed ST errata `ES0612` and applied the documented `VFQFPN32` workaround from section `2.2.9` for nonbonded GPIOs causing increased Run-mode current by forcing the listed nonbonded pins to pulldown at startup. That workaround had no effect on the Deepstop issue. The custom board’s `VFBSD / VLXSD / VDDSD / VDDRF` schematic and BOM appear close to the ST reference, so we are asking whether there are known WL33 low-power / SMPS / Deepstop pitfalls beyond errata `2.2.9` that could explain a persistent `~500 µA` floor or an apparent reset/restart on Deepstop entry instead of the expected `~4 µA`.
It almost seems like deepstop is resetting the pins to their reset value or something??
2026-05-08 2:32 AM
@machinehum wrote:We have a custom `STM32WL33CCV6` (`VFQFPN32`) board ??
Then you'll need to share your schematic!
How to write your question to maximize your chances to find a solution
Are you measuring with your ST-Link (or whatever) physically disconnected, and have you done a full power cycle (not just a reset) before measuring?
@machinehum wrote:similar to the NUCLEO-WL33??
Do you achieve 4uA on the Nucleo board?
@machinehum wrote:schematic and BOM appear close to the ST reference
How close is "close" ... ?
You need to show the schematic for people to be able to check!
2026-05-10 11:22 PM