cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL build error with CubeMX & IAR

edmond yun
Associate II

HI, 

please help to check the following build error.

I used CubeMX and IAR build tool and the following code.

en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node

 

Error is as below,

Error[Li005]: no definition for "BSP_RADIO_GetRFOMaxPowerConfig" [referenced from C:\work\stm_project\Lora_Test\
WLE5CC6_LORA\EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_GetTxConfig" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\
EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_ConfigRFSwitch" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\
EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_IsDCDC" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_Init" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_IsTCXO" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error while running Linker

Total number of errors: 6

 

thanks.

1 REPLY 1
STTwo-32
ST Employee

Hello @edmond yun 

I'm not able to reproduce this issue using the STM32CubeWL V 1.3.0, STM32CubeMX V6.12.1 and EWARM V9.60.2. Could you please update to those versions and ensure to download the SDK from our ST website.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.