2024-01-29 9:51 AM
Hello everyone, I hope you are well.
I'm working with the STM32WB55. I'm having difficulty getting RTC to work correctly.
The VBat is always powered by 3v3, I have an on/off switch that only removes the power from the VDD, however, when I turn it off and on the microcontroller is stuck in the routine: "while (LL_RCC_LSE_IsReady() == 0U)". I noticed that when CFG_HW_RESET_BY_FW is 1, the board continues to function, but it resets the RTC registers and the time is lost and when CFG_HW_RESET_BY_FW = 0, the firmware is stuck in the "while (LL_RCC_LSE_IsReady() == 0U)" routine. Looking through the oscilloscope, the clock is all right.
Can anyone help me? Thank you very much!
Solved! Go to Solution.
2024-02-07 4:25 AM - edited 2024-02-07 4:27 AM
Hello @ffjunq,
Kind Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-06 2:33 AM
Hello @ffjunq,
Thank you for your question !
Here some remarks :
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-06 5:42 AM
Hi Pierre, thank you very much for your support.
- I need to make my RTC never reset, so the VBAT is always in 3v3, remembering that I am using a V3 stlink to power the circuit. I have an on/off switch that only interferes with VDD, that is, VBat always 3v3.
- Following are the values of the registers:
- I don't need to charge the battery using VBat, as in the hardware I will use a specific chip to do this.
- In this case, I understand that the CFG_HW_RESET_BY_FW for my application always needs to be 0, so that it does not reset my RTC.
- Yes, I'm using CSS, but I've already tested with CSS off. And I'm not monitoring the VBat with the ADC, because I don't see the need for it at the moment, it may be that in the future I can use it to read the battery level, but I would have to check the possibility, since my battery is 4.2 V to 3V
- Yes, I have already read this document. However, I am performing again.
Thank you very much!
2024-02-06 10:30 AM
Taking advantage, I would like to know if there is a schematic of the ST, using a super capacitor so that the VBat is always at 3v3.
Thanks in advance!
2024-02-07 4:25 AM - edited 2024-02-07 4:27 AM
Hello @ffjunq,
Kind Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.