2020-01-29 01:04 PM
Hi,
I am trying to initiate a code via cubeMx for the STM32WB55.
I want to add freeRTOS together with a p2p_router capability but facing an issue that the both above not supported simultansly.
Any special reason for that?
Is there a way to achieve that?
Thanks.
2020-01-31 02:38 AM
I managed to reproduce your issue.
Unfortunately, the // support of many applications with free RTOS via CubeMX is under development as we target to support many other real time OS.
Meanwhile I would advise you to look at the project
STM32Cube_FW_WB_V1.4.0\STM32Cube_FW_WB_V1.4.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRateFreeRTOS
and use it as a reference to port the p2pRouter application on FreeRTOS.
2020-01-31 01:42 PM
Yeah I took that as last option, I hoped to find a better way than merge 2 demos cause than my cube file and source code are not consistent...
Thanks.