2020-07-19 11:26 AM
Hi,
I'm using CubeMX to generate the code for the STM32WB and I found a problem in the secuencer library which is automatically generated.
When I register a new task in the scheduler, this places the callback function in TaskCb[0] but when I set the task to be exectued the scheduler tries to trigger it from TaskCb[1] and this leads into a HardFault error.
I don't know if the problem is registering the tasks or exectuting them. Anyone else have seen this? Any ideas?
Working with the vesrion: STM32Cube FW_WB V1.4.0.
Regards,
Diego
2020-08-06 7:52 AM
First of all, could you try generate your code based on the latest releases V1.8 of the CubeWB FW package.
Looks like an error in the index computation.
2020-08-11 5:42 PM
Hi Remi,
Thanks for your answer. I've tried the latest release V1.8 but the scheduler still fails either registering the task or enabling it (see the image below)
I have uploaded the project to github but it's pretty much a copy/paste from the STM32WB Workshop video.
Ignoring the scheduler I can call the functions in different way but I guess if is there any bug you probably want to get it fixed.
Regards,
Diego
https://github.com/litanx/STM32WB55_BLE_Test
2020-08-13 5:00 AM
Hello,
The interface of the Sequencer requests a bit mask for all API.
In app_entry.c, you wrote
void HAL_GPIO_EXTI_Callback( uint16_t GPIO_Pin )
{
// switch (GPIO_Pin)
// {
// case BUTTON_SW1_Pin:
UTIL_SEQ_SetTask(1<<CFG_TASK_SW1_BUTTON_PUSHED_ID, CFG_SCH_PRIO_0);
//// break;
//// default:
//// break;
//// }
// return;
}
which is correct but in p2p_server_app.c, you wrote
void P2PS_APP_Init(void)
{
/* USER CODE BEGIN P2PS_APP_Init */
UTIL_SEQ_RegTask( CFG_TASK_SW1_BUTTON_PUSHED_ID, 0, P2PS_Send_Notification );
/* USER CODE END P2PS_APP_Init */
return;
}
which is not correct because you have been using the enum value and not the bit location.
It should be fixed this way
void P2PS_APP_Init(void)
{
/* USER CODE BEGIN P2PS_APP_Init */
UTIL_SEQ_RegTask( 1<<CFG_TASK_SW1_BUTTON_PUSHED_ID, 0, P2PS_Send_Notification );
/* USER CODE END P2PS_APP_Init */
return;
}
Generally speaking, the only way to get an HardFault with the Sequencer is to jump to a NULL callback.
There is most of the time only two reasons for this :
1/ The enum has been used in the interface whereas 1<<enum should have been used
2/ The interrupt that calls UTIL_SEQ_SetTask() is generated before UTIL_SEQ_RegTask() has been called to register the callback.
Regards.
2020-08-13 11:27 AM
Thanks for your help Christophe,
That actually have a lot of sense and looks kind of obvious now. It worked perfect with that change.
Regards,
Diego