2020-09-12 5:53 AM
Hi, i tried opening and debugging the STM32WB BLE-P2P example in my workspace but i dont get it to work. I tried a dozen ways to open and debug and even like in this video
https://www.youtube.com/watch?v=WgsXMVZfoO8&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=7&t=0s
but it doesn't work. One problem ist that the guy in the video seems to have different example files than these supplied by STM in github. And also code generation via new Project and then selecting existing examples in the IDE itself doesn't work.
Can you help me please
2020-09-12 5:55 AM
If i try it like in the video i get
14:43:17 **** Build of configuration Debug for project BLE_p2pServer ****
make -j12 all
make: *** No rule to make target 'C:/Utilities/lpm/tiny_lpm/stm32_lpm.c', needed by 'Utilities/stm32_lpm.o'. Stop.
"make -j12 all" terminated with exit code 2. Build might be incomplete.
14:43:17 Build Failed. 1 errors, 0 warnings. (took 488ms)
2021-07-31 12:24 AM
Hi,
did you fix that in the meantime. I run into the same problem. The only way I could fix it was to open the projects in the repository that comes with the firmware installation (usually c:\user\yourname\STMCube\Repository\...). The program is loaded correctly into the STMCubeIDE by double-click on the .project file. However, the files are not copied into your local workspace. They still located in the above mentioned repository. So everything you change changed there. At the moment the only way I found is to copy a lot of files manually from the repository to my project.
Best Regards
Markus
2022-11-17 3:36 PM
I'm having the same problem. So much value of examples is lost if it's too hard to clone them as a starting point for our own code.
I have tried copying the project file from the repository into my workspace and then copying all the driver and middleware folders into my file structure 2 levels above my workspace and adjusting the compiler and linker paths to match. That didn't work.
I have tried deleting the .project file and re-generated it from the .ioc file with CubeMX, and that didn't work.
I have successfully generated a new project with CubeMX that has some basic functionality, but of course it's missing all of the user code from the example, so that's not so useful. I'm going to try that again but then replace all the .c and .h files with the ones from the repository example.
It would be so great if ST would build their examples (including _ota versions) consistent with .ioc files in the project directory and with everything needed to clone the example in the project directory, so that I can just copy the project directory folder into my own workspace, put it under configuration control, build it and run it. Then start making my own changes to the .ioc file and user source code. Or describe some specific additional steps to get to the same point, where example code that was copied from the repository file structure to another location, builds and runs.
Back to my latest attempt, here are my steps:
2022-11-18 4:46 PM
O.k., now I need to modify this new project for OTA, following the directions in the readme of the BLE_p2pServer_ota example.
2023-03-28 11:46 AM
I got the same error when trying ST Example.
make: *** No rule to make target 'C:/........
The problem happened when creating the example project by double clicking ".project" or ".cproject" file in FW library. Instead, there would be no problem if creating the project through MX process: New, STM32 Project, Example Select ....
-wq
2024-04-04 8:13 AM - edited 2024-04-05 8:41 AM
I managed to solve it this way:
Step 4 I did mainly because the YouTube tutorial from ST told me to. I don't know if it helped avoid our problem.
EDIT: the code that you expect would be preserved, was in fact not copied to the new project location.
2024-06-24 2:01 AM - edited 2024-06-24 2:44 AM
When cloning or downloading the STM32Cube_FW_WB_V1.19.0 the examples comes with relative include paths (../)
Opening the Compiler Include Paths looks like this:
When copying a example project the resources should therefore be included as well. This is done in the .ioc file by enabling 'Copy only the necessary library files'.
Afterward the relative include paths should be changed to match the current include paths of the project.
Go to Properties > C/C++ Build > MCU GCC Compiler > Include paths. Update these acording to your project setup. The default setup that matches the folder structure of STM32Cube_FW_WB_V1.19.0 is shown on the first screenshot.
2024-11-26 6:52 AM
This thread was created on 2020-09-12. The problem is still there today !! even after 4 years STM is not able to resolve it !. It is the example project on eval kit and we were supposed to start from these.
2024-11-26 6:53 AM
This thread was created on 2020-09-12. The problem is still there today !! even after 4 years STM is not able to resolve it !. It is the example project on evaluation kit and we were supposed to start from these.