cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB getDescriptor UUID 2902 returns null

YGail.2
Associate III

I successfully implemented a service with different characteristics. However on the android side when I call getDescriptor()

descriptor =characteristic.getDescriptor(UUID.fromString(CLIENT_CHARACTERISTIC_CONFIG));
CLIENT_CHARACTERISTIC_CONFIG = "00002902-0000-1000-8000-00805f9b34fb";

It always returns null. I need this to set the notify command to be true. In the ST BLE Toolbox, this works perfectly. So in principle, this should be able to be called. It seems that I missed a setting in CubeMX.

1 ACCEPTED SOLUTION

Accepted Solutions
YGail.2
Associate III

I found probably why UUID 2902 is not callable. aci_gatt_add_char_desc() which in my opinion add the descriptor (UUID 2902) is never called. Hence I opened a new threat to this routine (https://community.st.com/s/question/0D53W000028ScADSA0/how-to-use-acigattaddchardesc-for-stm32wb-ble), as I could not find any documentation in the manual.

View solution in original post

3 REPLIES 3
Javier1
Principal

What languaje is this? is that code from your ST BLE mcu?

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

This is java on the android side. I could not call the given UUID from MCU. Hence I suppose that I missed something in CubeMx​

YGail.2
Associate III

I found probably why UUID 2902 is not callable. aci_gatt_add_char_desc() which in my opinion add the descriptor (UUID 2902) is never called. Hence I opened a new threat to this routine (https://community.st.com/s/question/0D53W000028ScADSA0/how-to-use-acigattaddchardesc-for-stm32wb-ble), as I could not find any documentation in the manual.