cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubewl_v1-2-0 HAL_ADCEx_Calibration_Start does not work

John1960
Associate II

In the middle of function returns HAL_ERROR.

stm32cubewl_v1-1-0 - the function works well.

12 REPLIES 12

I thought ADC_Enable() would be sufficient, but an initial test found this still returns the error on calibration.

MechMan
Associate II

Hi. I have this problem with stm32g07, but only -Og compile flag. The solution the same, Delay after Enable or use ADC_Enable

Dana Myers
Senior

is there a plan / what is the plan to roll out a fix for this? Using FW 1.3 I still see this.

Thanks -

Dana