2022-05-30 11:34 PM
In the middle of function returns HAL_ERROR.
stm32cubewl_v1-1-0 - the function works well.
Solved! Go to Solution.
2022-07-19 7:19 AM
Hello,
A regression has been introduced in release v1.2.0.
Issue:
In case of high frequency ratio between CPU and ADC (CPU high frequency, ADC low frequency), function HAL_ADCEx_Calibration_Start() returns an error.
Root cause:
A delay must be fullfilled between ADC enable and ADC disable.
Fix:
In function HAL_ADCEx_Calibration_Start(), a delay must be added:
LL_ADC_Enable(hadc->Instance);
<delay here>
LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
LL_ADC_Disable(hadc->Instance);
The fix will be available in next STM32WL FW package release.
Documentation is being updated to mention this constraint.
Best regards
Philippe
2022-05-30 11:37 PM
Sorry, MCU STM32WLE5
2022-06-06 1:17 AM
Hello and welcome @John1960 ,
You can have a look at the example ADC_AnalogWatchdog that you can find here :
STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Examples\ADC\ADC_AnalogWatchdog
In the main function there is a calibration that don't return an error.
Which code are you running ?
Best regards
2022-06-06 12:10 PM
I use my own code, which use ADC. First I want to calibrate it, so I call HAL_ADCEx_Calibration_Start.
I began from stm32cubewl_v1-1-0, and it worked well.
Then I upgaded library to stm32cubewl_v1-2-0, and the function began to return HAL_ERROR.
Functions HAL_ADCEx_Calibration_Start from version 1.1 and from version 1.2 are extreemly different.
Part of my code - Green LED is ON:
void ADC_Init ()
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_HSI;
if ( HAL_RCCEx_PeriphCLKConfig ( &PeriphClkInitStruct ) != HAL_OK )
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_ADC_CLK_ENABLE();
hadc.Instance = ADC;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = DISABLE;
hadc.Init.NbrOfConversion = 1;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
hadc.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
hadc.Init.OversamplingMode = DISABLE;
hadc.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/* ADC interrupt Init */
HAL_NVIC_SetPriority(ADC_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(ADC_IRQn);
// return;
if (HAL_ADCEx_Calibration_Start(&hadc) != HAL_OK)
{
/* Calibration Error */
GreenLED_On ();
Error_Handler();
}
} // ADC_Init
2022-07-19 7:19 AM
Hello,
A regression has been introduced in release v1.2.0.
Issue:
In case of high frequency ratio between CPU and ADC (CPU high frequency, ADC low frequency), function HAL_ADCEx_Calibration_Start() returns an error.
Root cause:
A delay must be fullfilled between ADC enable and ADC disable.
Fix:
In function HAL_ADCEx_Calibration_Start(), a delay must be added:
LL_ADC_Enable(hadc->Instance);
<delay here>
LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
LL_ADC_Disable(hadc->Instance);
The fix will be available in next STM32WL FW package release.
Documentation is being updated to mention this constraint.
Best regards
Philippe
2022-07-19 9:26 AM
OK
2022-09-09 5:07 PM
/* Apply calibration factor */
LL_ADC_Enable(hadc->Instance);
while (!LL_ADC_IsActiveFlag_ADRDY(hadc->Instance))
/* spin */;
LL_ADC_ClearFlag_ADRDY(hadc->Instance);
LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
LL_ADC_Disable(hadc->Instance);As above, I spin on ADRDY, no need for a timer
2022-09-11 8:24 AM
I reported the issue for STM32CubeWB as well.
The library already have some macros that wait for ADRDY the flag, just remove the LL_ prefix:
/* Apply calibration factor */
ADC_Enable(hadc);
LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
ADC_Disable(hadc);
2022-09-11 1:33 PM
Any notion of when the next STM32WL FW release will be available?
2022-09-21 3:28 PM
Holy crap - Same problem on STM32G030 chips.
The solution was posted two month ago.
Why you dont make a rollout about that?
I had searched a while to find that...
After calling the calibration function, the ADC_IT is stopped working.
No Hal_Error comes out.
@Dana Myers
Your spin cycle is running really great.
Thank you for posting that!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.