2023-11-06 01:06 AM
Hi, I am wondering if you can get STM32 MCU with integrated Bluetooth Classic as the only examples I have found (Like WB55) are all bluetooth low energy?
Solved! Go to Solution.
2023-11-06 10:01 AM - edited 2024-07-22 06:00 AM
Hello @Linkpad
ST is integrating the last BLE Technologie in the STM32WB series and specially in the STM32WBA series which include High data rate, long range, High output power and a Low-power messaging capability. I think that you can run almost all possible BLE applications using one of our MCUs. you can give as your project specification, and we may can guide you to a product that can do the job.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-06 10:01 AM - edited 2024-07-22 06:00 AM
Hello @Linkpad
ST is integrating the last BLE Technologie in the STM32WB series and specially in the STM32WBA series which include High data rate, long range, High output power and a Low-power messaging capability. I think that you can run almost all possible BLE applications using one of our MCUs. you can give as your project specification, and we may can guide you to a product that can do the job.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-22 04:35 AM
Sorry to wake an old thread, but this has come up a few times recently:
@STTwo-32 wrote:HI think that you can run almost all possible applications using one of our MCUs.
But not if your application needs to do Bluetooth Classic !
At the time of writing, with very few exceptions, that means pretty much anything with BT audio:
Another example would be the Classic Bluetooth Serial Port Profile (SPP):
https://www.bluetooth.com/specifications/specs/serial-port-profile-1-1/
(There is no standard "serial port" profile for BLE - but plenty of proprietary implementations)
2024-07-22 04:56 AM
I can confirm this. Thank you so much for this feedback @Andrew Neil . I've already mentioned that it implements BLE technologie.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-22 05:44 AM
@STTwo-32 wrote:I've already mentioned that it implements BLE technologie.
Indeed.
But what people don't seem to realise is that this excludes BT Classic - and that most BT audio is, in fact, BT Classic.
Hence I think, "you can run almost all possible applications using one of our MCUs" needs some qualification.
2024-07-22 06:00 AM
I've updated this.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.