cancel
Showing results for 
Search instead for 
Did you mean: 

se-identity.h

SWenn.1
Senior III

I have a node connected to a gateway and a chirpstack server.  I decided I want to understand a few topics.  So I went into the above file and changed the EUI from a working 80,00,00,00,00,00,00,06 to below. 

#define LORAWAN_JOIN_EUI                                   A0,01,B0,02,C0,03,D0,04

 I rebuild code and the node still works with the network server which has listed the 80....EUI number.

I am running the node as OTAA but cannot understand why the new EUI won't take.  Can someone please explain how to make this work?

1 REPLY 1
STTwo-32
ST Employee

Hello @SWenn.1 

I suggest you try to disconnect and reconnect the Node with new parameters. That may do the Job.

Best regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.