2022-07-07 12:45 AM
Can anyone confirm if it is okay to supply the RF switch directly from a general purpose output of the STM32WL? This way I could control when the switch is working or when the antenna is isolated (off) from the circuit.
I see in the datasheet for the STM32WL that "The GPIOs can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH)". While for the RF switch the typical supply current is of 65uA and a maximum of 110uA.
Seems that it should be okay. Could anyone that has done this or anyone with the knowledge confirm this is a good practice?
Thanks and best regards,
Asier
Solved! Go to Solution.
2022-07-08 3:08 AM
Hello,
Yes, it is perfrectly fine to control RFSwitch through GPIOs.
This is what is done on stm32wl nucleo board (https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html)
You can find an implementation of the control in stm32cubewl (https://www.st.com/en/embedded-software/stm32cubewl.html) in the ATSlave application example.
BR,
Benoit
2022-07-07 1:30 AM
Well, ST's own B-L072Z-LRWAN1 board supplies its TCXO from a port pin - so it should be fine to supply just an RF switch...
2022-07-08 3:08 AM
Hello,
Yes, it is perfrectly fine to control RFSwitch through GPIOs.
This is what is done on stm32wl nucleo board (https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html)
You can find an implementation of the control in stm32cubewl (https://www.st.com/en/embedded-software/stm32cubewl.html) in the ATSlave application example.
BR,
Benoit