cancel
Showing results for 
Search instead for 
Did you mean: 

Restore ST-Link Connection on B-L072Z-LRWAN1

Andrew Neil
Evangelist III

In order to achieve minimum power drain on the B-L072Z-LRWAN1 discovery board, it is necessary to remove some solder bridges

See:

https://community.st.com/s/question/0D50X00009XkbSOSAZ/excess-current-consumption-running-bl072zlrwan1-from-battery

And:

https://community.st.com/s/question/0D50X00009q4M1zSAE/cant-power-bl072zlrwan1-with-battery

To be able to use the onboard ST-Link again, these connections need to be restored:

  • NRST: link CN4.3 to CN12.5;
  • SWD: fit two links on CN8;
  • VCOM: link CN5.1,2 to JP6.

0693W00000NpgutQAB.jpg 

Rather than have to mess about with 2 separate links for the SWD, a single-row 4-pin header can be adapted:

0693W00000Npgv3QAB.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Evangelist III

It wasn't a question - just posting a tip.

View solution in original post

1 REPLY 1
Andrew Neil
Evangelist III

It wasn't a question - just posting a tip.