cancel
Showing results for 
Search instead for 
Did you mean: 

Repeatedly failing BLE firmware update due to FUS_IMAGE_WRTERROR.

DPars.2
Associate III

I'm running FUS 1.2.0 on an STM32WB55CEU and every time I try to update the BLE firmware over USB I get a FUS image write error. It appears to download and verify successfully but always fails during the actual firmware update. I can't seem to find this error anywhere else on the forum (or Google) so am I the only one having this issue?

 08:58:38 : ST-LINK error (DEV_CONNECT_ERR)

 08:58:45 : USB speed  : Full Speed (12MBit/s)

 08:58:45 : Manuf. ID  : STMicroelectronics

 08:58:45 : Product ID : DFU in FS Mode

 08:58:45 : SN     : 205536685841

 08:58:45 : FW version : 0x011a

 08:58:45 : Board    : --

 08:58:45 : Device ID  : 0x0495

 08:58:45 : UPLOADING OPTION BYTES DATA ...

 08:58:45 :  Bank     : 0x00

 08:58:45 :  Address    : 0x1fff8000

 08:58:45 :  Size     : 128 Bytes

 08:58:45 : UPLOADING ...

 08:58:45 :  Size     : 1024 Bytes

 08:58:45 :  Address    : 0x8000000

 08:58:45 : Read progress:

 08:58:45 : Data read successfully

 08:58:45 : Time elapsed during the read operation is: 00:00:00.024

 08:58:49 : FUS state is FUS_IDLE

 08:58:49 : FUS status is FUS_NO_ERROR

 08:58:51 : Deleting firmware ...

 08:58:52 : Firmware delete finished

 08:58:52 : Firmware delete execution finished

 08:58:53 : Connection to device 0x495 is lost

 08:58:53 : Disconnected from device.

 08:58:54 : ST-LINK error (DEV_CONNECT_ERR)

 08:58:57 : USB speed  : Full Speed (12MBit/s)

 08:58:57 : Manuf. ID  : STMicroelectronics

 08:58:57 : Product ID : DFU in FS Mode

 08:58:57 : SN     : 205536685841

 08:58:57 : FW version : 0x011a

 08:58:57 : Board    : --

 08:58:57 : Device ID  : 0x0495

 08:58:57 : UPLOADING OPTION BYTES DATA ...

 08:58:57 :  Bank     : 0x00

 08:58:57 :  Address    : 0x1fff8000

 08:58:57 :  Size     : 128 Bytes

 08:58:57 : UPLOADING ...

 08:58:57 :  Size     : 1024 Bytes

 08:58:57 :  Address    : 0x8000000

 08:58:57 : Read progress:

 08:58:57 : Data read successfully

 08:58:57 : Time elapsed during the read operation is: 00:00:00.025

 08:59:01 : Download Stack/FUS image at address 0x8053000 ...

 08:59:01 : Memory Programming ...

 08:59:01 : Opening and parsing file: stm32wb5x_BLE_Stack_full_fw.bin

 08:59:01 :  File     : stm32wb5x_BLE_Stack_full_fw.bin

 08:59:01 :  Size     : 183536 Bytes

 08:59:01 :  Address    : 0x08053000 

 08:59:01 : Erasing memory corresponding to segment 0:

 08:59:01 : Erasing internal memory sectors [83 127]

 08:59:02 : Download in Progress:

 08:59:06 : File download complete

 08:59:06 : Time elapsed during download operation: 00:00:04.813

 08:59:06 : Verifying ...

 08:59:06 : Read progress:

 08:59:10 : Download verified successfully 

 08:59:10 : FUS state is FUS_IDLE

 08:59:10 : FUS status is FUS_NO_ERROR

 08:59:13 : Firmware Upgrade process started ...

 08:59:13 : Updating firmware ...

 08:59:13 : Waiting for firmware upgrade end

 08:59:17 : FUS state is WIRELESS_STACK_UPGRADE_ONGOING

 08:59:17 : FUS status is FUS_IMAGE_WRTERROR

 08:59:17 : Firmware upgrade Error!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
DPars.2
Associate III

Well, I didn't really find the root cause but I've at least found a work around. All the failures were happening when I tried to update through USB DFU. I was also powering the board through USB. This board also has test point access to the SWD pins so I changed my set-up to power the board with an external power supply and connect STM32CubeProgrammer via SWD and now it programs successfully. There is obviously some sort of hardware issue with my USB connection.

View solution in original post

2 REPLIES 2
DPars.2
Associate III

Same failure from command line and option bytes...

0693W00000HpGqIQAV.png0693W00000HpGqXQAV.png

DPars.2
Associate III

Well, I didn't really find the root cause but I've at least found a work around. All the failures were happening when I tried to update through USB DFU. I was also powering the board through USB. This board also has test point access to the SWD pins so I changed my set-up to power the board with an external power supply and connect STM32CubeProgrammer via SWD and now it programs successfully. There is obviously some sort of hardware issue with my USB connection.