2021-12-20 7:40 AM
I'm running FUS 1.2.0 on an STM32WB55CEU and every time I try to update the BLE firmware over USB I get a FUS image write error. It appears to download and verify successfully but always fails during the actual firmware update. I can't seem to find this error anywhere else on the forum (or Google) so am I the only one having this issue?
08:58:38 : ST-LINK error (DEV_CONNECT_ERR)
08:58:45 : USB speed : Full Speed (12MBit/s)
08:58:45 : Manuf. ID : STMicroelectronics
08:58:45 : Product ID : DFU in FS Mode
08:58:45 : SN : 205536685841
08:58:45 : FW version : 0x011a
08:58:45 : Board : --
08:58:45 : Device ID : 0x0495
08:58:45 : UPLOADING OPTION BYTES DATA ...
08:58:45 : Bank : 0x00
08:58:45 : Address : 0x1fff8000
08:58:45 : Size : 128 Bytes
08:58:45 : UPLOADING ...
08:58:45 : Size : 1024 Bytes
08:58:45 : Address : 0x8000000
08:58:45 : Read progress:
08:58:45 : Data read successfully
08:58:45 : Time elapsed during the read operation is: 00:00:00.024
08:58:49 : FUS state is FUS_IDLE
08:58:49 : FUS status is FUS_NO_ERROR
08:58:51 : Deleting firmware ...
08:58:52 : Firmware delete finished
08:58:52 : Firmware delete execution finished
08:58:53 : Connection to device 0x495 is lost
08:58:53 : Disconnected from device.
08:58:54 : ST-LINK error (DEV_CONNECT_ERR)
08:58:57 : USB speed : Full Speed (12MBit/s)
08:58:57 : Manuf. ID : STMicroelectronics
08:58:57 : Product ID : DFU in FS Mode
08:58:57 : SN : 205536685841
08:58:57 : FW version : 0x011a
08:58:57 : Board : --
08:58:57 : Device ID : 0x0495
08:58:57 : UPLOADING OPTION BYTES DATA ...
08:58:57 : Bank : 0x00
08:58:57 : Address : 0x1fff8000
08:58:57 : Size : 128 Bytes
08:58:57 : UPLOADING ...
08:58:57 : Size : 1024 Bytes
08:58:57 : Address : 0x8000000
08:58:57 : Read progress:
08:58:57 : Data read successfully
08:58:57 : Time elapsed during the read operation is: 00:00:00.025
08:59:01 : Download Stack/FUS image at address 0x8053000 ...
08:59:01 : Memory Programming ...
08:59:01 : Opening and parsing file: stm32wb5x_BLE_Stack_full_fw.bin
08:59:01 : File : stm32wb5x_BLE_Stack_full_fw.bin
08:59:01 : Size : 183536 Bytes
08:59:01 : Address : 0x08053000
08:59:01 : Erasing memory corresponding to segment 0:
08:59:01 : Erasing internal memory sectors [83 127]
08:59:02 : Download in Progress:
08:59:06 : File download complete
08:59:06 : Time elapsed during download operation: 00:00:04.813
08:59:06 : Verifying ...
08:59:06 : Read progress:
08:59:10 : Download verified successfully
08:59:10 : FUS state is FUS_IDLE
08:59:10 : FUS status is FUS_NO_ERROR
08:59:13 : Firmware Upgrade process started ...
08:59:13 : Updating firmware ...
08:59:13 : Waiting for firmware upgrade end
08:59:17 : FUS state is WIRELESS_STACK_UPGRADE_ONGOING
08:59:17 : FUS status is FUS_IMAGE_WRTERROR
08:59:17 : Firmware upgrade Error!
Solved! Go to Solution.
2021-12-21 1:45 PM
Well, I didn't really find the root cause but I've at least found a work around. All the failures were happening when I tried to update through USB DFU. I was also powering the board through USB. This board also has test point access to the SWD pins so I changed my set-up to power the board with an external power supply and connect STM32CubeProgrammer via SWD and now it programs successfully. There is obviously some sort of hardware issue with my USB connection.
2021-12-20 9:00 AM
Same failure from command line and option bytes...
2021-12-21 1:45 PM
Well, I didn't really find the root cause but I've at least found a work around. All the failures were happening when I tried to update through USB DFU. I was also powering the board through USB. This board also has test point access to the SWD pins so I changed my set-up to power the board with an external power supply and connect STM32CubeProgrammer via SWD and now it programs successfully. There is obviously some sort of hardware issue with my USB connection.