2024-06-19 11:05 PM
Can anyone tell me how to do it without wasting days to simply compile a project from the repo:
https://github.com/STMicroelectronics/STM32CubeWB
although if I import any ìxample from stm32cubeide when I compile it tells me that there are missing libraries, the same thing if I import the IOC, in short it is impossible to work like this!!!!!!!!!!!
I lose a lot of days!
Can you give me a screenshot of the steps to follow!!
Solved! Go to Solution.
2024-06-20 12:09 AM
Hello @battellino and welcome to the ST Community
The reason behind his problems may be that you have downloaded the STM32CubeWB package from the GitHub repository directly using the "download zip" button and not the git command:
git clone --recursive https://github.com/STMicroelectronics/STM32CubeWB.git
I suggest you try using the Cube package downloaded from the ST website or the one cloned from the Git repository using the command I've shared.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-20 12:09 AM
Hello @battellino and welcome to the ST Community
The reason behind his problems may be that you have downloaded the STM32CubeWB package from the GitHub repository directly using the "download zip" button and not the git command:
git clone --recursive https://github.com/STMicroelectronics/STM32CubeWB.git
I suggest you try using the Cube package downloaded from the ST website or the one cloned from the Git repository using the command I've shared.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-20 01:13 AM
Thanks , I try .
Another problem:
Im running ble heart of stm32wb55 , I would like use adc input channel with the ADC_SingleConversion_TriggerTimer_DMA_ but the tim2 that i instantiate seem not run; the variable ubDmaTransferStatus that indicate the end of dma tranfert(value = 1) is right to insert in callback in the main or in hrs_app.c????
2024-06-20 02:06 AM
This is a new question. If your original question is answered, close this topic by selecting a best answer and create a new post for this question to give it more visibility.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.