Skip to main content
Visitor II
December 4, 2023
Solved

Hardware/fuse disabling OTA updates for security?

  • December 4, 2023
  • 1 reply
  • 1081 views

Hi All!

We have a requirement to disable OTA updates either via hardware or by settings a fuse, this is due to the need for a low-maintaince, low-complexity, high-security method to prevent updates to those without physical access to the device.

Is there a fuse or fuses that can be used for this purpose? Or maybe a PIN that can be used for this?

We're looking to disable the OTA (aka FUOTA) for the STM32WLE5CBU6 which is listed as OTA capable in the datasheet.

Thanks all! :D

 

 

This topic has been closed for replies.
Best answer by STTwo-32

Hello @billyjoel 

There is no way to do that. FUOTA is purely software and does not check hardware settings.

Best Regards.

STTwo-32

 

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
June 20, 2024

Hello @billyjoel 

There is no way to do that. FUOTA is purely software and does not check hardware settings.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.