2023-02-11 4:58 PM
Hello I have two STM32WL55JC2 boards and I would like to run the PingPong DualCore example available in this WL package folder :
I run the .project file on the STM32 IDE and I get this:
After adding several missing .h files I manage to flash to the boards but I think I am missing a step.
In the tutorial it says:
"
- Open your preferred toolchain
- Rebuild all CM4 files and load your image into CM4 target memory
- Rebuild all CM0PLUS files, set PWR_CR4_C2BOOT flag via CM4 and load your image into CM0PLUS target memory
- Do the same for second board
- Reset the two boards
- Run the example on two boards
- Open two Terminals, each connected to their respective PingPong Device
- UART Config = 115200, 8b, 1 stopbit, no parity, no flow control
"
It's not working from now on and i think i've missed something but i can't find what.
"Rebuild all CM0PLUS files, set PWR_CR4_C2BOOT flag via CM4 and load your image into CM0PLUS target memory" i don't know how to do this line if someone can help me !
if anyone has a simple video to start this example i would be very happy !
Thank you
Solved! Go to Solution.
2023-02-14 1:01 AM
Hello @BNamu.1 ,
There is several videos explaining how to deal with dual core projects on STM32WL. You can access them here !
I hope this will help you
Regards
Louis
2023-02-14 1:01 AM
Hello @BNamu.1 ,
There is several videos explaining how to deal with dual core projects on STM32WL. You can access them here !
I hope this will help you
Regards
Louis