2020-09-08 05:45 AM
I have bought this product set.
I can connect to its gateway through virtual serial Tera terminal. Also it can connect to Loriot gateway server.
However, the sensor node board with the USI I-NUCLEO-LRWAN1 shield does not respond to AT command through a Tera terminal. Also, the Cayene application does not show any activity of this sensor board.
How do I correct it?
Solved! Go to Solution.
2021-01-23 10:57 AM
A bit late, but:
"the sensor node board ... does not respond to AT command through a Tera terminal"
Note that this is to be expected: as the Getting Started Guide tells you, the ST-Link UART is disconnected from the target on the Nucleo board.
See my post of January 20, 2021 at 12:05 PM in this thread:
https://community.st.com/s/question/0D53W00000DHlVaSAL/i-want-to-get-pnucleolrwan2-gateway-source
2021-01-23 10:57 AM
A bit late, but:
"the sensor node board ... does not respond to AT command through a Tera terminal"
Note that this is to be expected: as the Getting Started Guide tells you, the ST-Link UART is disconnected from the target on the Nucleo board.
See my post of January 20, 2021 at 12:05 PM in this thread:
https://community.st.com/s/question/0D53W00000DHlVaSAL/i-want-to-get-pnucleolrwan2-gateway-source