2021-09-19 12:41 PM
The sample code from the library worked out of the box. I tried to generate similar code via CubeMX.
I tried to set the parameter "radio_bord_if -> Select radio Driver"myself, because without this, the CubeMX issues a warning.
However, when building the project, I get incomprehensible errors regardless of the value of this parameter.
I didn't find the radio_fw.c anywhere other than the AN5687 description, so I deleted it from the project.
After that I got an error: " Error[Pe136]: struct "LmHandlerCallbacks_s" (declared Hat line 135 of "...Repository/STM32Cube_FW_WL_V1.0.0/Middlewares/Third_Party/LoRaWAN/LmHandler\LmHandler.h"h) has no field "GetUniqueId" ...\Project_WL\LoRaWAN_End_Node\LoRaWAN\App\lora_app.c 134 " that I don't understand either.
Solved! Go to Solution.
2021-09-20 8:47 AM
I apologize! The issue was resolved by copying the library from the official site. Bad library came to me after updating the CubeMX.
2021-09-20 8:47 AM
I apologize! The issue was resolved by copying the library from the official site. Bad library came to me after updating the CubeMX.