2021-03-10 6:17 AM
I followed this[1] URL to update FUS and wireless stack, it failed and now i can't get wireless to work. All the examples are hard faulting. My FUS is still in version 0.5.3
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x20030030
0x20030030 : 00050300
But i can't upgrade to the latest one.
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in FS Mode
SN : 206F3169554D
FW version : 0x011a
Device ID : 0x0495
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
Current FUS Version : 0x00050300==================] 100%
Uploaded FUS Version : 0x01000200
FUS state is FUS_IDLE
FUS status is FUS_NO_ERROR
Old wireless stack delete ...
Deleting firmware ...
Firmware delete finished
FUS state is FUS_SERVICE_ONGOING
FUS status is FUS_IMAGE_NOT_FOUND
FUS state is FUS_IDLE
FUS status is FUS_NO_ERROR
Download firmware image at address 0x80ec000 ...
Memory Programming ...
Opening and parsing file: stm32wb5x_FUS_fw_1_0_2.bin
File : stm32wb5x_FUS_fw_1_0_2.bin
Size : 24492 Bytes
Address : 0x080EC000
Erasing memory corresponding to segment 0:
rasing internal memory sectors [236 241]
erasing sector 0236 @: 0x080ec000 done
erasing sector 0237 @: 0x080ed000 done
erasing sector 0238 @: 0x080ee000 done
erasing sector 0239 @: 0x080ef000 done
erasing sector 0240 @: 0x080f0000 done
erasing sector 0241 @: 0x080f1000 done
Download in Progress:
[==================================================] 100% 4%
File download complete
Time elapsed during download operation: 00:00:00.487
FUS state is FUS_IDLE
FUS status is FUS_NO_ERROR
Firmware Upgrade process started ...
Updating firmware ...
Waiting for firmware upgrade end
FUS state is WIRELESS_STACK_UPGRADE_ONGOING
FUS status is FUS_NO_ERROR
FUS state is WIRELESS_STACK_UPGRADE_ONGOING
FUS status is FUS_IMAGE_NOT_AUTHENTIC
Error: Firmware not authentic!
How do i get my bluetooth back up and running?
[1]: https://github.com/ARMmbed/mbed-os/blob/master/targets/TARGET_STM/TARGET_STM32WB/README.md
Solved! Go to Solution.
2021-03-11 8:07 PM
Fixed this by first erasing all sectors from the "Erasing and programming" section of the programmer GUI and then flashing the FUS by
STM32_Programmer_CLI -c port=usb1 -fwupgrade stm32wb5x_FUS_fw_1_0_2.bin 0x080EC000 firstinstall=0
2021-03-10 7:04 AM
Or is it possible to flash the original wireless stack that came with the board?
2021-03-11 8:07 PM
Fixed this by first erasing all sectors from the "Erasing and programming" section of the programmer GUI and then flashing the FUS by
STM32_Programmer_CLI -c port=usb1 -fwupgrade stm32wb5x_FUS_fw_1_0_2.bin 0x080EC000 firstinstall=0