2024-07-07 10:38 AM - last edited on 2024-07-08 06:59 AM by Amel NASRI
Hello everyone,
I want to measure the current consumption on a STM32WB5MMDK discovery board. I've found that I had to put an ammetre on the jumper JP1, and I programmed the RGB LED to be working. However, when I put the ammetre and I power my board, I found that the current is null, and I can't find why, even if I checked the schematics and the datasheets. I was supposed to have something around 100 mA normally.
Does anyone know the reason of my problem ?
Thank you
Nour
2024-07-07 10:55 AM - edited 2024-07-07 11:00 AM
Show foto or read p14 Discovery kit with STM32WB5MMG module - User manual
2024-07-08 12:57 AM
Yes, that is what i have followed.
I am joining the pictures
2024-07-08 01:17 AM
Hi,
your DMM is on AC ... 🙂
press function, to set DC measurement .
Then you will see...