cancel
Showing results for 
Search instead for 
Did you mean: 

More bugs in CubeIDE code generation for STM32WL33

divmstr
Associate III

When generating code that uses the CMSIS OS V2, it appears that a template directory gets included in the generated code. causing massive linker errors. 

The offending directory is Drivers/CMSIS/Device/ST/DEM32WL3X/Source/Templates. Removing it gets rid of the errors.

While we are at it, the LICENSE.txt file in the same directory is spelled incorrectly, it should be LICENCE.txt, as it is not a verb.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @divmstr 

I'm not able to reproduce this behavior. Could you please test it using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and give me the file that reproduce this issue if it is reproduced on your side.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @divmstr 

I'm not able to reproduce this behavior. Could you please test it using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and give me the file that reproduce this issue if it is reproduced on your side.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.