2021-06-11 06:13 AM
Hi,
I am using LoRa-E5 mini board from seeed studio (https://www.seeedstudio.com/LoRa-E5-mini-STM32WLE5JC-p-4869.html)
To program it using STM32CubeIDE, do we need to connect it to pc using ST-Link or we can simply program it via Type C cable?
Solved! Go to Solution.
2021-06-15 07:46 AM
Hi @FBrin.1 ,
Sorry for the delay to answer you, as this period is very busy for me with many tasks.
You need to connect the ST-LINK to a target using the SWD cable as you can see below.
You can check the SWD pins connections in the UM1075, Table 4. JTAG/SWD cable connections.
I hope this helps !
Imen
2021-06-11 08:46 AM
Hello @FBrin.1 ,
Connect the STM32WLE5 board to the computer with a USB cable type C to the Type C port for power and serial communication, and connect another micro USB cable to the ST-Link side to the SWD pins.
You can refer to this resources for more help:
Hope this help you!
When your question is answered, please close this topic by choosing Select as Best.
Imen
2021-06-11 09:08 AM
Thanks Imen,
Can you please clarify this part : "connect another micro USB cable to the ST-Link side to the SWD pins."
Where can I get this ST-Link cable?
2021-06-15 02:57 AM
Hi @Imen DAHMEN
Can you please clarify this part : "connect another micro USB cable to the ST-Link side to the SWD pins."
Which ST-Link cable should be connected to SWD pins?
Will this work ? https://www.adafruit.com/product/2548
2021-06-15 07:46 AM
Hi @FBrin.1 ,
Sorry for the delay to answer you, as this period is very busy for me with many tasks.
You need to connect the ST-LINK to a target using the SWD cable as you can see below.
You can check the SWD pins connections in the UM1075, Table 4. JTAG/SWD cable connections.
I hope this helps !
Imen
2021-06-15 08:19 AM
Thanks @Imen DAHMEN
Will this be compatible? https://www.adafruit.com/product/2548
2021-06-15 08:26 AM
Yes, it is compatible. You can use it.
Imen
2021-06-17 04:03 AM
Hello
You discussed about hardware issue but you didn't talk about the more important!!!! how to make an End Node LORAWAN object that make join and send data to network with the STM32WLE5J8I for example.
NO information and no help on this subject!!!
2021-06-17 07:43 AM
2021-06-17 08:18 AM
Thank you for your answer but i want an example for the STM32WLE5J8I and the Nucleo use the STM32WL55 and it's not the same thing!!!