2022-08-19 3:03 AM
Hello,
I used a GFSK configuration with 433MHz and it is work very well,
I try now to migrate to Lora modulation. i used a basic config, but the receiver on the other side receive less then 1% of sent frames ! (even transmitter and receiver are very close)
is anybody has advice to improve communication ?
Solved! Go to Solution.
2022-09-01 1:11 AM
finally i resolved the problem :
in fact, i made an application without hal drivers, just ll drivers. so, i have write my own code to interface radio drivers with subghzSPI inspired by hal_subghz.
but for some reason, it worked on GFSK modulation but no in LoRa modulation.
finally, i implemented hal_subghz file and necessary definitions to run it, and it is working done :)
2022-08-19 3:46 AM
I finally found that the lack of detection is not due to Lora configuration.
but my receiver (I dont know why) receive a hardfault interruption after receiving !
it is not the case for the transmitter
I always need your help, maybe i have messed something in receiver config !
2022-08-19 5:32 AM
last update after multiple debugging :
1 - when i set fix payload length in tx and rx config, i have a crc error in detected frame, i detect wrong data, than a hardfault.
2 - when i set variable payload length, i don't have the hardfault, but a cannot detect all frame (less then 1% are detected) and when i detect, i usually have a header error
i set the same config for the transmitter and the receiver.
2022-08-22 6:21 AM
I tried to configure lora modulation on an other way, but always the same problem !
pleas find the code below
2022-08-24 8:08 AM
Hello @malarab ,
Can you try with an example project from STM32Cube_FW_WL_V1.2.0, like SubGHz_Phy_PingPong to see if you achieve to make it work with LoRa modulation in 433MHz.
Don't forget to add this line in "subghz_phy_app.h" to select the right frequency :
#define REGION_EU433
Let me know the result
Best regards
Louis
2022-08-25 12:49 AM
Hi Loius,
Thank you for your answer
1 - Yes, PingPong example is working,
2 - I have resolved the problem of HardFault : in fact i do not use HAL drivers, so i programmed my own low-level code, i missed some callback function for LoRa (because i do not use them in GFSK). putting these function again the HardFault problem is resolved.
3 - I steel have problem on receiving : i cannot receive all sent frames !
4 - I am sur that transition is ok, because i detect all data with PingPong receiver.
I am reviewing my low level code to verify that all is ok ...
2022-09-01 1:11 AM
finally i resolved the problem :
in fact, i made an application without hal drivers, just ll drivers. so, i have write my own code to interface radio drivers with subghzSPI inspired by hal_subghz.
but for some reason, it worked on GFSK modulation but no in LoRa modulation.
finally, i implemented hal_subghz file and necessary definitions to run it, and it is working done :)