cancel
Showing results for 
Search instead for 
Did you mean: 

Issue after unplug/replug during operation

Tony_Tony
Associate II

Hi,

I'm working with the nucleo-wb15cc board. The program itself is working great but I encounter issues everytime I unplug/replug the USB cable during operation:

The program reports HAL_TIMEOUT druing SystemClock_Config(). To be more specific, it gets stucked in the while loop here:

 

 

/* Check the LSE State */ if (RCC_OscInitStruct->LSEState != RCC_LSE_OFF) { /* Get Start Tick*/ tickstart = HAL_GetTick(); /* Wait till LSE is ready */ while (LL_RCC_LSE_IsReady() == 0U) { if ((HAL_GetTick() - tickstart) > RCC_LSE_TIMEOUT_VALUE) { return HAL_TIMEOUT; } } } else......

 

 

I see from the clock diagram that LSE is involved in RTC Clock Mux and RFWKP Clock Mux.

BOOT0 is pulled to GND according to schematic.

I figured out a way to go around the issue, of which I also don't understand the mechanism: by flashing the Heart_Rate example codes and reflashing my own codes, the program can run again without any issues. However, I need to reflash my codes twice because I'll get a hard fault after the first reflash. It works again after the second reflash.

My application: collecting data with ADC, using DMA with sampling rate defined by HAL_TIM, update Bluetooth characteristic in ADC_Cplt_Callback by sending the 12-bit ADC-value in 2 seperate bytes. I used the timer from HW_TS to have 5ms between each update. HSE&LSE: both bypass clock source. 

Have a nice day :)

1 ACCEPTED SOLUTION

Accepted Solutions
Tony_Tony
Associate II

The issue is solved when I use external oscillator for HSE&LSE. But I would prefer to use internal oscillator to save power and have less wiring. Is it still possible? 

View solution in original post

1 REPLY 1
Tony_Tony
Associate II

The issue is solved when I use external oscillator for HSE&LSE. But I would prefer to use internal oscillator to save power and have less wiring. Is it still possible?