cancel
Showing results for 
Search instead for 
Did you mean: 

I am using a NUCLEO-WL55JC1 and the LoRaWAN_End_Node example. I want to add USART1 to the example, so that I can forward the UART data over LoRa. The problem is that the interrupts for USART1 never trigger if the LoRaWAN process is also running.

BBI Louw
Associate

If I comment out "MX_LoRaWAN_Process();" in main, then the USART1 interrupts trigger as they normally would. Could anyone offer some advice of how to add USART1 to the example?

Kind regards

1 REPLY 1
Ma_05
Associate II

Sorry for the question but have you correct your problem because I have the same