2019-03-22 7:15 PM
(1) We use our own custom board with the STM32WB55RGV6, we want to test the radio.
Question:
Is the CPU2 CM0+ already programmed with the "stm32wb5x_BLE_Stack_fw.bin" from the factory?
I have tried to download the "stm32wb5x_BLE_Stack_fw.bin" using ST-Link Utility and with assistance of a STM32WB Nucleo board, with address: 0x080CB000. The firmware download process was successful, no error message shown.
(2) We have tested the board, by downloading a blink LED firmware to the CPU1 CM4F, it works well.
(3) We also have tried to download the example "BLE_HeartRate" firmware, but the BLE is not detected by the ST BLE Sensor Mobile Application and by the ST BLE Profile App.
Questions:
Is there any document or instruction on how to do further tests, especially the radio portion?
What kind of tools needed?
Should we use STM32CubeMonitor-RF app?
Any comment, question back, or feedback would be greatly appreciated.
Best wishes,
Edy Gunawan
.
2019-03-22 7:28 PM
The schematic is as below:
2019-03-23 4:55 AM
To update the firmware on CPU2 CM0+, do the following:
(1) Connect the Boot0 pin to VDD
(2) Using command line: STM32_Programmer_CLI.exe -c port=usb1 –fwdelete
(3) Next, write command:
STM32_Programmer_CLI.exe -c port=usb1 -fwupgrade stm32wb5x_BLE_Stack_fw.bin 0x080CB000 firstinstall=1
Result:
After that:
(1) put back the Boot0 pin to low (pulled down by 10K resistor to GND)
(2) connect to Nucleo board's ST-Link (SWDIO, SWCLK, NRST, GND, VDD 3.3)
(3) Use ST-Link Utility to flash the CPU1 CM4F with BLE_beacon binary
Check using ST BLE Sensor app, the beacon is still not found.
Any further analysis ?
2020-03-06 10:14 PM
We are also facing the same problem!
Tried all these procedures, but no sign of BLE working.
Could anyone please guide us through initializing BLE in a fresh STM32WB controller?
2020-11-01 7:15 AM
Me too. I used a 3GHz spectrum analyser and found nothing output from the RF pin at all after going through all the FW flashing.
Appreciate if anyone can share their experience.
2020-11-03 1:14 AM
There are a lot of contributions on this community that explains the steps to program the STM32WB microcontroller.
Usual questions: What is the programming port used?
Could you download the option bytes?
Which tool do you use to flash the board. CubeProgrammer in GUI or CLI mode?
2020-12-18 9:52 PM
Try the following using STM32CubeProgrammer GUI
For more details instructions, please say so.
2023-01-08 11:10 PM
I tried this step on my Custom Board also but I stuck on Step 3, BTW, I use stm32WB55CC. Do you have any particular settings for this chip? any help would be appreciated.
Im starting to doubt that maybe I should just use BLE module interfaced in UART instead of WB MCus. :sad_but_relieved_face: