2022-05-20 02:29 AM
Hello ST,
During the provisioning in mesh network a node address assigned by PROVISIONER. which is going to be stored in LPN node memory.
-----------------Debug Trace-----------
BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfully
BLEMesh_PvnrDataInputCallback - Device Key: d4 ac c7 95 da 3c 8a 1d b7 dc d6 a0 50 3f fa a9
BLEMesh_PvnrDataInputCallback - App Key: e3 c5 54 9d d1 19 bf 00 56 80 9a 54 6a 54 e1 04
BLEMesh_PvnrDataInputCallback - Node Address Assigned = 3
Device is provisioned by provisioner
----------------------------------------------------------
i want to delete this "Node Address Assigned = 3" from the LPN memory without system reset. so i can reuse this number again from provisioner side.
Best Regards
Deepak Aagri
Solved! Go to Solution.
2022-05-25 01:56 AM
Hello,
The only way to delete the "Node Address Assigned = 3" is to unprovisione the provisioner node and provision again the network.
Best Regards
2022-05-25 01:56 AM
Hello,
The only way to delete the "Node Address Assigned = 3" is to unprovisione the provisioner node and provision again the network.
Best Regards