cancel
Showing results for 
Search instead for 
Did you mean: 

How to enable the BLE Custom template with the FreeRTOS running?

ABN
Associate III

The project is running on FreeRTOS in the CMSIS_V2 mode.

I need to have a BLE custom template to configure my own services and characterisctics.

In the case with the FreeRTOS running, I can just enable the BLE SIG Heartrate. The other BLE Applications are not present. But, if I disable the RTOS, then all the BLE applications are available.

Is there any way to enable both RTOS and the BLE Custom template?

Thanks in advance.

MCU used: STM32WB55

Dev board: P-Nucleo WB55

0 REPLIES 0