2021-06-15 2:30 AM
Hi,
I am using demo board "NUCLEO-WL55JC1" to run SubGHz_Phy_PingPong example.
if I did not change anything, I can see the message, the default usart RX and TX is PA3 and PA2.
123s023:Rx start
125s023:OnRxTimeout
125s025:Master Tx start
125s216:OnTxDone
125s219:Rx start
127s219:OnRxTimeout
127s221:Master Tx start
127s413:OnTxDone
127s416:Rx start
129s416:OnRxTimeout
129s417:Master Tx start
now I want to configurate PB7 and PB6 to see the message, how do I do ?
Could you give me some advice , please?
Solved! Go to Solution.
2021-06-15 3:11 AM
Hello,
Please look into usart.c and usart_if.c files and update them to use usart1 instead of usart2.
Change stm32wlxx_it.c as well to add USART 1 IRQ.
2021-06-15 3:11 AM
Hello,
Please look into usart.c and usart_if.c files and update them to use usart1 instead of usart2.
Change stm32wlxx_it.c as well to add USART 1 IRQ.
2021-06-15 6:28 PM
Hi Mike,
Thanks for your reply.
Is there any manual about how interrupt function is called in stm32wlxx_it.c?
2021-06-15 11:11 PM
Hi Mike,
I can see the message after configurate PB7 and PB6 now, thanks.
I have other question:
I am using demo board "NUCLEO-WL55JC1" to run SubGHz_Phy_PingPong example, I can see some message.
Can I run this example with a board designed by the STM32WLE5JB MCU?
I tried, but I can not see any message, I don't know why? (my board is using PB7 and PB6 as RX and TX too.)
but when I use “..\Examples\DMA\DMA_MUXSYNC\MDK-ARM�? example to run on my board , I can see message, so I am sure the hardware is good.
Messagge as follow:
This example shows how to use the DMA with the DMAMUX to synchronize a transfer with LPTIM1 output signal.
The USART1 is used in DMA synchronized mode to send a countdown from 10 to 00 with a period of 2sec
Start countdown :
10
09
08
07
06
05
04
03
02
01
00
Example Finished
My board is using PB7 and PB6 as RX and TX too. so I modified PB7 and PB6 as RX and TX in SubGHz_Phy_PingPong example, and I can see
message when I flash firmware to demo board "NUCLEO-WL55JC1",
why do I not see any message when I run SubGHz_Phy_PingPong example on my board ?
Could you give me some advice, please?
2021-06-16 1:14 AM
Hello,
Hard to tell.
Check with debugger whether the software is hanging somewhere.
2021-06-16 6:10 PM
Hi Mike,
So the SubGHz_Phy_PingPong single core example can compatible with STM32WLE5JB MCU, right?
I am using the source code from en.stm32cubewl.zip for STM32WLE5JB MCU, is it right?
"Check with debugger whether the software is hanging somewhere."
====Could you tell me how to use debugger, please? any manual?
====Do I need to modify some macro in source code?
On the other hand, I found that:
If I select stm32wle5jb mcu in SubGHz_Phy_PingPong single core example and compile ,then flash fw to NUCLEO-WL55JC1 demo board , it keeps going round and round in follow source code line 1821. Do you know why?
2021-06-18 1:06 AM
Hi Mike,
My board is working well with SubGHz_Phy_PingPong single core example, I change RCC_RTCCLKSOURCE_LSE to RCC_RTCCLKSOURCE_LSI since my board has no LSE clk.
Thank you all the same.
but I met other problem. when I am using two board(demo board and my board) to test , I always see the messae "OnRxError".
could you give me some advice ,please?
debug message:
1s541:Rx start
RBI_ConfigRFSwitch config = 1
1s617:PRE OK
1s634:HDR OK
1s728:OnRxDone
1s728:RssiValue=-76 dBm, SnrValue=2
RBI_ConfigRFSwitch config = 0
1s730:OnRxError
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 3
1s734:Master Tx start
RBI_ConfigRFSwitch config = 3
1s911:OnTxDone
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 4
1s914:Rx start
RBI_ConfigRFSwitch config = 1
1s991:PRE OK
2s008:HDR OK
2s102:OnRxDone
2s102:RssiValue=-76 dBm, SnrValue=1
RBI_ConfigRFSwitch config = 0
2s104:OnRxError
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 3
2s108:Master Tx start
RBI_ConfigRFSwitch config = 3
2s285:OnTxDone
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 4
2s288:Rx start
RBI_ConfigRFSwitch config = 1
2s365:PRE OK
2s382:HDR OK
2s476:OnRxDone
2s476:RssiValue=-76 dBm, SnrValue=2
RBI_ConfigRFSwitch config = 0
2s478:OnRxError
RBI_ConfigRFSwitch config = 0
2021-06-18 7:18 AM
Hello,
please read the readme.txt for the SubGHz_Phy_PingPong project, I understand you need 2 boards to make it work.
2021-06-20 5:57 PM
Hello Mike,
I know I need two boards to test.
I test SubGHz_Phy_PingPong project between Two demo board(NUCLEO-WL55JC1), working well.
but when I test SubGHz_Phy_PingPong project between demo board(NUCLEO-WL55JC1) and my board, my board displays message as follow:
1s541:Rx start
RBI_ConfigRFSwitch config = 1
1s617:PRE OK
1s634:HDR OK
1s728:OnRxDone
1s728:RssiValue=-76 dBm, SnrValue=2
RBI_ConfigRFSwitch config = 0
1s730:OnRxError
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 3
1s734:Master Tx start
RBI_ConfigRFSwitch config = 3
1s911:OnTxDone
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 4
1s914:Rx start
RBI_ConfigRFSwitch config = 1
1s991:PRE OK
2s008:HDR OK
2s102:OnRxDone
2s102:RssiValue=-76 dBm, SnrValue=1
RBI_ConfigRFSwitch config = 0
2s104:OnRxError
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 3
2s108:Master Tx start
RBI_ConfigRFSwitch config = 3
2s285:OnTxDone
RBI_ConfigRFSwitch config = 0
PingPong_Process state = 4
2s288:Rx start
RBI_ConfigRFSwitch config = 1
2s365:PRE OK
2s382:HDR OK
2s476:OnRxDone
2s476:RssiValue=-76 dBm, SnrValue=2
RBI_ConfigRFSwitch config = 0
2s478:OnRxError
RBI_ConfigRFSwitch config = 0