2022-05-30 1:28 AM
Hello
I have a P-NUCLEO-LRWAN3 kit. I would like to apply some peripheral at Gateway but I didn't find the source code.
If I can't get the gateway source code. I would like to get the binary pre-installed on the NUCLEO-WRWAN3 gateway.
Thank you.
2022-05-30 8:59 AM
Hello,
You can find the firmware of the gateway here. You can choose between Actility and Loriot providers to their respective network servers.
Best regards
Louis
2022-05-31 12:55 AM
Thank you for your reply.
I tried to download Loriot provider firmware, but the link you provided is just Loriot's main page. I couldn't find any further information.
So I searched the Loriot page to get the gateway firmware, but couldn't find any information on how to download the firmware.
Is there something I'm missing about that?
Thank you.
2022-06-01 2:23 AM
Hello,
That's right I did not notice, I look for a link to allow you to download those firmware.
First, you can download the gateway firmware for TTN and Loriot here.
You can configure it to point to Loriot network server, or to change the frequency, thank to this documentation UM2587.
Refer to the section 6 to configure your gateway.
I will add the Actility gateway firmware soon.
Hope it help
Best regards
Louis
2022-06-01 2:48 AM
For the Actility firmware, once you are connected, you can go in the Base Stations tab, Create, and once you choose STMicroelectronics manufacturer and your model, you can download the base station image.
You have also a direct link here.
Best regards
2022-07-29 4:32 AM
Is C codes of P-NUCLEO-LRWAN3 published? how can i reach C codes?
2022-08-17 12:29 AM
2023-03-30 6:21 AM
Hello,
Is the software for the gateway published? I am pretty sure it is not, but I wanted to be sure. I wanted to store the data comming through the gateway locally, but it seems like you can only change a few parameters using AT commands.
Kind regards,
Thines
2023-05-09 6:59 AM
Hello, I even could not find the LORIOT firmware package ? Is there anyone to inform how can I find it ?
Thanks
2023-05-12 12:22 AM
Well, the URL was given in the previous answer. There you will find the tab Tools & Software, where you will also find the reference to the LORIOT gateway firmware under Embedded Software from Partners.
Finally, you will come on the LORIOT website, where you can register free of charge and download the firmware as a binary.
Please direct all questions regarding LORIOT to the partner LORIOT.
Regards
/Peter