2020-02-15 1:13 AM
I have a Nucleo pack. I loaded the Bluetooth test files (.HEX) into the main board and the dongle that comes in the pack and the code is working as explained. However when I compiled (Hex code not provided) and loaded ZigBee code, the unit is displaying error by all three LEDs flashing (as per manual). I thought the ZigBee binary might not have loaded and tried to check. ST has provided a Command Line Interface (CLI) program to read/program the co-processor. When I try to read the FLASH of the co-processor, I am getting only 00s, though I disable read protection. I would like to first check if ZigBee binary is loaded or not and if it is not loaded I would like to load it. Can someone help me in this regard please? Thank you for your time.
2020-02-15 1:18 AM
Which product are you talking about?
2020-02-15 11:07 AM
The product is STM32WB55RG Nucleo board. It is a set containing one nucleo board and a dongle.
Thanks.
2020-02-20 6:33 PM
Hi all,
Feels as if I am in wilderness!!! Is there no one who can help me?? Thank you.