2019-04-09 12:35 PM
Using either the default program or programming the BLE_TransparentMode default hex file results in this error. I have both a windows 10 and macOS 10.14.4 machine that I get this result. The VCOM port doesn't seem to be the issue as I can program and see the units. Any help would be much appreciated!
2019-04-10 6:46 AM
Hello BGoathals
This error usually means that tool has no answer from device. In this case the log will look like this :
The tool has tried to contact the target, but there was no answer after few seconds.
There could be various causes for this :
There is an overview of the connection in the user manual (UM2288, chapter 2) You may find some clues in this doc, and it should help to understand the connection path.
Best regards
2019-10-25 5:27 AM
Hello @stephane.legargeant ! I think this problem concerns to me too. But to use the transparent mode? I'm using stm32wb55 and I want to connect it with my phone.
2020-07-09 6:19 AM
@BGoathals @stephane.legargeant @Kolab Have you found any solution to the problem, e.g. how to set a transparent mode?
2020-07-09 11:39 AM
@MPiot.1 I really forgot how I overcame this issue(issues were a lot :) ) but I get an idea. On the STM32CubeWB folder look for the folder BLE_TransparentMode and look at the readme, it may help.
2020-07-09 12:25 PM
@Kolab Thank you for your reply. The point is I cannot find the mentioned folder, as well as I do not see the directory containing the examples, which could be also helpful.
2020-07-09 1:22 PM
just type on the browser STM32CubeWB
clicking on the st link you will redirected to the download page
2020-07-10 12:38 AM
@Kolab Found it, but even uploading the recompiled binary does not work, CubeMonitor RF does not find the COM port at all. Would you e so nice to share any working project file?
2020-07-10 1:44 AM
Hello MPiot.1
As indicated by @Kolab , the software "transparent mode" delivered in STM32CubeWB. For a Nucleo board, it is in Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_TransparentMode
What board are you using ? Nucleo, USB dongle or custom board ?
You should check that computer detects the virtual com port : i.e. for windows, check in device manager if the com port is detected.
Stephane
2020-07-10 1:55 AM
Dear @stephane.legargeant I am using STM32WB55 Nucleo board. I activated the Virtual Port Com in project configuration and it is detected both in Windows Device Manager and in CubeMonitor-RF but when clicking "connect" button I receive the warning "Could not open COM port".