cancel
Showing results for 
Search instead for 
Did you mean: 

cube-lrwan execution error

MWisi.1
Associate II

Sir,

I testing the STM32L0 + SX1276 with en.i-cube_lrwan_v2.1.0 lib

I compiled the AT COMMANDS example on KEIL and then with STM32 IDE too, but during execution i am always getting the following error in both

APP_VERSION:    V1.1.0

MW_LORAWAN_VERSION: V2.3.0

MW_RADIO_VERSION:  V1.1.0

0s000:error: The Region is not defined in the MW: set lorawan_conf.h accordingly

it´s weird, because in lorawan_conf.h i defined

/* Region ------------------------------------*/

/* the region listed here will be linked in the MW code */

/* the application (on sys_conf.h) shall just configure one region at the time */

/*#define REGION_AS923*/

#define REGION_AU915

/*#define REGION_CN470*/

/*#define REGION_CN779*/

/*#define REGION_EU433*/

/*#define REGION_EU868*/

/*#define REGION_KR920*/

/*#define REGION_IN865*/

/*#define REGION_US915*/

/*#define REGION_RU864*/

Some tip ?

0693W00000Hqo9AQAR.png 

Thank you!!!!!

4 REPLIES 4

Going to have to pay more attention to what that define pulls in vs other ones that work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MWisi.1
Associate II
MWisi.1
Associate II

Now running on WISOL LOM204