cancel
Showing results for 
Search instead for 
Did you mean: 

Costum board stuck at PeriphCommonClock_Config();

matsmort
Associate II

hi,

 

Im using my own costum board with a STM32WBA52CG on it. When I'm nog using the RF my code is working perfectly. When I activate the RF in the STM32CubeIDE, my code is stuck in  PeriphCommonClock_Config();

More specifically in the following code:

Screenshot 2024-05-07 at 17.34.13.png

 I already checked my HSE crystal and I'm getting 32 MHz out. So what could be wrong? because without the RF I'm not able to use BLE..

 

 

Thanks in advance!

 

Kind regards,

 

Mats 

1 ACCEPTED SOLUTION

Accepted Solutions

I did not attach the antenna yet, thats why it got stuck on that line! 

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @matsmort 

Could you share your .ioc file.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi,

 

it is already solved!

 

kind regards,

 

mats

Happy to know that. Could you please share the solution. That may help other users.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I did not attach the antenna yet, thats why it got stuck on that line!