cancel
Showing results for 
Search instead for 
Did you mean: 

Connect multiple identical BLE devices to Windows

amit_ble
Associate

I am using the STM32WB55 microcontroller for my product. I want to connect more than one module to my Windows laptop. When I pair one module, it pairs correctly, but when I try to connect another module with the same firmware, it shows the message "Try to connect your device again" and does not connect. I have tried changing many things, but it is still not working. Where do I need to make changes so I can connect both devices with the same firmware to my laptop?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @amit_ble 

This depends on the tolerated number of connections on the central side (your PC). And not on the STM32WB side (that will be the peripheral).So, please check the capability of your BLE module (on the PC).

 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @amit_ble 

This depends on the tolerated number of connections on the central side (your PC). And not on the STM32WB side (that will be the peripheral).So, please check the capability of your BLE module (on the PC).

 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.