2024-12-16 05:03 AM - last edited on 2024-12-16 05:12 AM by Andrew Neil
I am using the STM32WB55 microcontroller for my product. I want to connect more than one module to my Windows laptop. When I pair one module, it pairs correctly, but when I try to connect another module with the same firmware, it shows the message "Try to connect your device again" and does not connect. I have tried changing many things, but it is still not working. Where do I need to make changes so I can connect both devices with the same firmware to my laptop?