2024-07-15 09:02 PM
How can I make sure that the the router and server should work in a pair with no cross connection. Now I know both of these work as I can see on ST toolbox but how can I check if the are connected among them selves . I earlier modified an example to trigger data transmission using push button . I am able to understand the server but I have no idea what and how can I deal with router. I need this router to accept data from Server . add some more data to it and then share it to my phone.
I am currently using two stm 32wb5mm DK one as a server and other as a router.