2024-06-18 11:44 PM - last edited on 2024-06-19 3:10 AM by Peter BENSCH
Hello.
I am developing a BLE HID device using the STM32CubeWB MCU Firmware Package, but when I try pairing => disconnect => pairing, pairing fails.
I have an implementation like this, is there a problem?
We have the following data in adv_data, which should not exceed 31 bytes (we have confirmed Success)
Also, if I put a breakpoint before aci_gap_update_adv_data, I can re-pair successfully. (I guess that means the timing of aci_gap_update_adv_data is NG?)
I would be grateful if you could give me an answer. Thank you.
Solved! Go to Solution.
2024-06-19 12:11 PM
Hello @ELEHM and welcome to the ST Community :smiling_face_with_smiling_eyes:.
From the context, we can see that there have been issues with the handling of bonding information and the updating of advertising data in the past. For instance, there was a mention of a problem where the second call to aci_gap_update_adv_data() always failed, returning an error code due to length data problems.
Additionally, there was a discussion about the need to wait for a certain amount of time after receiving the EVT_DISCONN_COMPLETE event before turning off the STM32WB or performing certain operations to ensure that the bonding information is properly stored. So, I suggest you add a delay of more than 100ms after receiving the disconnection event before initiating any further actions.
So, I suggest you to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-19 12:11 PM
Hello @ELEHM and welcome to the ST Community :smiling_face_with_smiling_eyes:.
From the context, we can see that there have been issues with the handling of bonding information and the updating of advertising data in the past. For instance, there was a mention of a problem where the second call to aci_gap_update_adv_data() always failed, returning an error code due to length data problems.
Additionally, there was a discussion about the need to wait for a certain amount of time after receiving the EVT_DISCONN_COMPLETE event before turning off the STM32WB or performing certain operations to ensure that the bonding information is properly stored. So, I suggest you add a delay of more than 100ms after receiving the disconnection event before initiating any further actions.
So, I suggest you to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-19 10:27 PM - edited 2024-06-19 10:29 PM
Hello.@STTwo-32
With your help, I was able to successfully pair a second time by adding a delay right after the disconnect event. (It's written in the API library, sorry I didn't look closely enough...)
Thank you very much!
Best Regards.