cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f746disco board repair

Fish
Associate II

hi,

i have purchased the stm32f746 disco board recently

the disco board stlink connection is in fail, after the i have shorted 5V - GND (big big big mistak..)

i found that this led(LD7) control is in charge st-link mcu (stm32f103)

LD7 Red LED is toggled when i powered on this board

##what does mean this?##

i've checked wave form of m7 oscillator and rtc clock and stm32f103 clock (st-link) using scope

also, 5V to 3V3 power logic is ok

##is this mcu (stm32f7) dead?##

--------------------------------------------------------------------------------------------------

stupid..

now i can use disco board again.. thanks

cable short was not problem

just usb hub was something worng

none of the pars have not been dead

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
MM..1
Chief III

shorted 5V - GND cant kill board, you maybe short some other too ...

Fish
Associate II

thank you for replying to me

well, after the logic was shorted, i have eliminated cable lines on board

----------------------------------------------------

LD7 Red LED Toggle notify users something is wrong

but, now i can access to mcu using st link

S.Ma
Principal

If usb power source is a hub or a pc, it has overcurrent protection (imagine the pc breaks when shorting 5v and gnd through external device, would overwhelm support). Usually there are protection to limit returns to manufacturers...

Fish
Associate II

thanks :)