cancel
Showing results for 
Search instead for 
Did you mean: 

[BLE] Get number of current connected devices

DS.4
Senior II

After going through AN5270, I have a few questions.

I realize that there can be up tp 2 connection to slave.

Can I read the current list of connected devices ( not yet paired) from the stack via an HCI/ACI command?

As for LIMITED_DISCOVERY command can TGAP be changed to a lower value than 180 sec?

2 REPLIES 2
Remy ISSALYS
ST Employee

Hello,

You can use ACI_HAL_GET_LINK_STATUS command, this command returns the status of the 8 Bluetooth low energy links managed by the device.

Best Regards

DS.4
Senior II

@Remy ISSALYS  Thnanks,

Regarding the LIMITED_DISCOVERY, is there a way to change the TGAP?

Or, a different command that will have a timeout event?