cancel
Showing results for 
Search instead for 
Did you mean: 

Writing characteristic fails with bad parameter

jimmy11
Associate

Hello all,

Working on communication between two STM32WB55 boards , one configured as client , and one as server.

When trying to write a characteristic I get a bad parameter error, but when I use the write characteristic long command it works fine.

Writing a small amount of bytes works on both commands.

MTU discussed: 0xFB > size of write ( 0x5E).

 

What can be the issue?

 

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @jimmy11 

Are you sure of this information:

  • MTU discussed: 0xFB

Best regards .

II

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @jimmy11 

Are you sure of this information:

  • MTU discussed: 0xFB

Best regards .

II

Thanks, when I used the the MTU exchange command it solved the issue

Happy to now that you're problem has been solved.

Please close the topic by choosing a best answer.

Best regards.

II