2023-01-14 2:51 PM
After going through AN5270, I have a few questions.
I realize that there can be up tp 2 connection to slave.
Can I read the current list of connected devices ( not yet paired) from the stack via an HCI/ACI command?
As for LIMITED_DISCOVERY command can TGAP be changed to a lower value than 180 sec?
2023-01-16 6:38 AM
Hello,
You can use ACI_HAL_GET_LINK_STATUS command, this command returns the status of the 8 Bluetooth low energy links managed by the device.
Best Regards
2023-09-11 6:43 AM
@Remy ISSALYS Thnanks,
Regarding the LIMITED_DISCOVERY, is there a way to change the TGAP?
Or, a different command that will have a timeout event?