Hello
We would like to evaluate your STM32WBA55G and nucleo-WBA55CG boards for a project. So we have several questions:
- Is it possible to stream BLE audio between two STM32WBA55G boards by taking the sound from the Mems microphone and streaming it to the pc via the USB port (We could see the live audio of the audacity) If so, what examples should we use in your codes?
- Is it possible to do the same thing but having the nucleo connected to the PC and which to recover the audio in BLE. We would have the card STM32WBA55G further away that would be streaming the audio by picking up the audio from its microphone
- Is it possible to connect a STM32WBA55G to an nRF5340 Audio via BLE audio?
- When will you have the final documentation for the software and hardware of the STM32WBA55G board?
Kind regards