2023-06-29 7:43 AM
I have a dev_kit which I want to use to connect to a cellular network with LTE-M. But the example-file that they gave were a .bin file from XCUBE_CELLULAR for B-L462E-CELL1\cellular. Since I never used i, I have no clue what to do. How could I get started with the modem and get a connection with a network. So that I can send and receive data? OR something like the project-example they gave to us. That would also help.
Thank you!
2025-01-21 8:21 AM
Hey,
I am also currently working with the same board and am kinda lost. Did you had any progress or update on your work?
Thanks