cancel
Showing results for 
Search instead for 
Did you mean: 

2.4GHz frequency band support

leahjoseph
Associate II

Hello,

I am looking for a low power STM32 MCU that can transmit 2.4GHz RF signals. Since STM32WBA and STM32WB support bluetooth, can it be used to transmit raw 2.4GHz signals as well as bluetooth.

It is used to communicate with a cnc controller.

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @leahjoseph

The STM32WB/WBA support multiple protocols that are Bluetooth® Low Energy 5.4, IEEE 802.15.4 communication protocols, Zigbee, Thread and Matter.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @leahjoseph

The STM32WB/WBA support multiple protocols that are Bluetooth® Low Energy 5.4, IEEE 802.15.4 communication protocols, Zigbee, Thread and Matter.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.